2021-12-07 11:42 AM
Gooday
I have a steering wheel which has buttons programmed with an stm32 blue pill board.... my problem is
The board is only recognised on my pcs front USB ports ......any USB ports on the back side of the board give an error (cannot recognise and ports reset failed )...please is there a specific driver I need or how can I fix this
2021-12-07 12:49 PM
Wouldn't that indicate a problem with your USB ports rather than a problem with the STM32 board?
2021-12-07 2:38 PM
While waiting for more useful answers:
Get a powered USB 2.0 hub (high speed or full speed, not USB 3.x) and connect your device thru it.
Unless your PC runs Windows 7. Then upgrade :)
2022-01-26 5:38 AM
I have the exact same problem seems its something to do with the STM32 board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.