STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CLASS-B STL Run-time FLASH CRC Error, the test staus is TEST_RUNNING mode only not comming to Test_OK

i have integrated STL XCUBE class-B 2.2.0 Packages with STM32L433 controller here iam facing the test its always TEST_RUNNING not comming to Test_OK stauts, i am getting Run-time FLASH CRC Error, what could be the issue.  #define ROM_START ((uint32_t...

Ssiva.2 by Associate II
  • 3080 Views
  • 3 replies
  • 0 kudos

uSD card write operation stops after some time.

Hello everyone,I am student and using the FATFS middleware to log sensor data to a uSD card using stm32f746g dev board. The data gets logged only for the first few minutes (8 minutes) and then the f_write() returns a status as FR_LOCKED (16).What cou...

SGupt.7 by Associate II
  • 2230 Views
  • 3 replies
  • 0 kudos

Resolved! How to use the mutex RTOS .

Hi, I want to synchronize the my threads execution using the mutex.here is my code /*---------------------------------------------------------------------------- * CMSIS-RTOS 'main' function template *-----------------------------------------------...

Trinu by Associate III
  • 5899 Views
  • 3 replies
  • 0 kudos

Resolved! Example or guide to use LwIP PPPos ?

Hi,we are starting to learn about LwIP in order to create a http server in a stm32f4. At this moment we have a functional hardware that act as http client using a modem with AT Commands (the quectel MC60). However, now we have been asked to create a ...

DCajigal by Associate III
  • 4747 Views
  • 2 replies
  • 0 kudos

Resolved! Application not loading after DFU:Leave

I am trying to program the STM32F401 flash on our board in DFU mode. I am using the dfu-util tool in my Linux computer.I am using the following code to flash and jump to application code.dfu-util -a 0 -s 0x08000000:leave -D <location-to-binary>.binAf...

PA.3 by Associate
  • 3925 Views
  • 1 replies
  • 5 kudos

Question about CMSIS driver

I've download the CMSIS pack for STM32H7 series. ST implement an I2C driver function like this:​int32_t I2C_MasterTransmit (uint32_t addr, const uint8_t *data, uint32_t  num, bool  xfer_pending, I2C_RESOURCES *i2c), ​but the website, https://arm-soft...

JLee.32 by Associate III
  • 4417 Views
  • 8 replies
  • 0 kudos

STM32F407VET6 Custom Board Ethernet not working

Hello, F407VET TQFP100 on custom board, ethernet PHY LAN8742A, STMCUBEIDE 1.6.1 on Linux (mint). PHY and MCU both clocked by 25MHz oscillator, reference clock 50MHz is OK. Cpu running @168MHz FREERTOS 3 task: default init LWIP, start HTTPD thread t...

0693W00000CzxZ5QAJ.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.