2014-01-15 10:14 AM
I�m trying to use the STM32F407 as Host and Device simultaneously, my hardware configuration is the following:
-PA12, PA11, PA9 OTG FS as a Device - PB14, PB15 OTG HS as a Host with Embedded PHY If I define the preprocessor symbols: USE_USB_OTG_HS and USE_USB_OTG_FSThe USB works ok as a Host, and the Device goes on and off, It seems that it is going to work but at the end the computer doesn't recognize it. Also, I have tested defining just the preprocessor macro USE_USB_OTG_FS, and in this case the USB works well as a Device. I believe that the library is only implemented to work in HS or FS ModeSo, this is my question, Does any body has implemented USB as a device and host simultaneously using separated peripheral ? I mean i want to use the HS as Host with no external PHY and the FS as a Device. #stm32f4 #usb #usb #usb #usb #stm32f407 #otg #host #host2014-03-13 6:11 AM
Hi Bompart.Romy,
Can you help us about using mix USB OTG HS HOST and USB OTG FS DEVICE with ST USB OTG library?2015-09-24 3:26 AM
Hi bompart.romy,
i
'm studyingfor my
university thesis
the
USB
-
OTGand I would be
interested in your
project
.You can
send it
by mail
?It would need
to understand
some of the settings
of the USB
-
OTG for STM32f407.
Thank you :)
2018-05-20 3:35 AM
Hi Bompart.Romy,
I also need help implementing a USB OTG HOST and USB OTG DEVICE with the ST USB OTG library.
In my case I need the USB HS operating as the device, and the FS as the USB host.
I have each working separately from the Device CDC standalone and Host HID standalone application examples.
My merge has the mouse working with USB HID FS, but only the first ASCIII text from my PC is received and responded to by the EVAL board on the USB HS (CDC VCP peripheral).
Can you help please?
2018-05-21 4:55 AM
HI cakali.anil,
Was Bompart.Romy able to help you about using mix USB OTG HS HOST and USB OTG FS DEVICE with ST USB OTG library?
I have a similar task.
2018-05-21 4:57 AM
Hi Ragazzi.Valerio,
Was Bompart.Romy able to help you about using mix USB OTG HS HOST and USB OTG FS DEVICE with ST USB OTG library?
I have a similar task.
Thanks
2018-05-21 5:07 AM
Hi Steven,
It would be better to create a new thread in which you describe the issue you're facing.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.