2012-06-15 3:32 AM
Where is the USBDM and USBDP (pins name for USB) defined under standard library files from stm. I have a microcontroller with USBDM and USBDP as PA11 and PA12. I would like to know in which header file the corresonding pins are defined as USBDM and USBDP.
I would be happy if someone could help me on this. Regards, #usbdp #usbdm2012-06-15 5:24 AM
I don't understand the question.
The pins are defined and fixed by the hardware, and the alternate function mapping.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.