STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data dropout in VCP USB application

Posted on June 27, 2012 at 05:20Hi,I am working on a vibration sensor project where I need to send data from an accelerometer over USB to a computer application with a data loading of about 24 bytes per millisecond. I am using using a custom-built S...

Pygmt OS is recruiting open source contributors

Posted on June 26, 2012 at 08:07Hi, my name is Warren Greenway, founder of Pygmy OS and the Pygmy Project. We are currently looking for a few good developers to join the core team in preparation for our first stable public release. Pygmy OS is an RT...

warrend by Associate
  • 1048 Views
  • 2 replies
  • 0 kudos

USB Mass Storage Demo Problems

Posted on September 20, 2011 at 21:51Hi,I am working with the STM3210C-EVAL Board and the demos provided with the STM32F105/7 and STM32F2xx USB on-the-go Host and device library.The libraries provided for initializing the USB on the device take a st...

USB input pins

Posted on June 15, 2012 at 12:32Where is the USBDM and USBDP (pins name for USB) defined under standard library files from stm. I have a microcontroller with USBDM and USBDP as PA11 and PA12. I would like to know in which header file the corresondin...

USB (VCP) failure when using a hub

Posted on June 11, 2012 at 01:22Hi, I've not been able to find any information on this issue so here goes... I am using an STM32F10x micro with the USB Virtual Com Port (STM32F10x USB-FS-Device Driver V3.3.0 and earlier versions) library. I have wor...

DFUse not reading device

Posted on April 10, 2012 at 15:29Hi, I am working with an STM32F4, and I am trying to use the USB OTG capability to boot load the flash drive. I have successfully loaded the flash trough UART3 using Flash Loader Demonstrator. In order to start the b...

Audio on STM32F4

Posted on May 25, 2012 at 15:55 Hi guys ! Firstly - hello to everyone ! I have some questions. I am trying to make a project on STM32F407VG that would transfer data from microphone to the headphones through a filter. I am totally new to t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.