2023-02-14 6:59 AM
Hello everyone
I am struggling with my custom board to be used as HOST or DEVICE.
In my board I have both connectors USB HOST A, and miniUSB Device connector in parallel.
When using an application as USB HOST for an USB Keyboard, everything is working fine.
When I am reprogram the application to be used as USB DEVICE CDC ACM Virtual Com Port it does not show in Linux, and there are a lot of error trying to connect and at least it fails loading USB Device. The device is HOST ONLY or DEVICE ONLY depends on which application I set. There is NO USD_ID pin connected as it works only for OTG/Dual Role stuff.
The hardware REMAINS the same. There are 2 22R Ohm resistor as impedence matching for lenght, and the lenght for each DATA LINE (D+ and D-) is less than 5 cm from the MCU.
The MCU is running with an external crystal/oscillator 8MHZ 49-HC style oscillator.
What can be checked to ensure the correct behaviour of the USB bus?
Regards,
Gianluca
2023-02-14 9:40 AM
so, if i get you right: same board, 2x software, host is working fine, device - does nothing.
my first idea: do you pull up dp+ by 1k5 to 3v3 ? (this is : hello host, here i am .)
or does your cpu this ? (see in rm...maybe.) or just try with a 1k5 soldered to dp+ and see...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.