2021-07-08 2:07 AM
Hello,
when using Linux host for testing this example, CDC interface is not detected by the host. Reason is sensitivity on Configuration descriptor content generated by STM32CubeMX, propagated into ux_device_descriptors.c. For now you fix this file manually if you want to verify example functionality with Linux host in ux_device_descriptors.c (~line 806)
/* Control interface headers */
pHeadDesc = ((USBD_CDCHeaderFuncDescTypedef *)((uint32_t)pConf + *Sze));
/* Header Functional Descriptor*/
pHeadDesc->bLength = 0x05;
pHeadDesc->bDescriptorType = 0x24;
pHeadDesc->bDescriptorSubtype = 0x01; //originally 0x00
pHeadDesc->bcdCDC = 0x0001; //originally 0x1001
*Sze += (uint32_t)sizeof(USBD_CDCHeaderFuncDescTypedef);Fix shall be propagated into future version of STM32CubeMX.
2021-07-08 4:31 AM
Thanks, that works.
The only thing that might be confusing for the unwary is that the Enter key may (depending on the terminal program one uses) only send a CR (Ctrl-M), if one wants the output to move to the next line, one has to explicitly send a LF (Ctrl-J) in that case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.