2017-06-24 10:07 AM
I am using cubemx v4.21.0. and the freertos version is 8.2.3. & the cmsis-rtos version is 1.02.
I am using the examples of STM32F413ZH-Nucleo in stm32cube F4 v1.16.0 , when I download the program. It works wrong!
I found the issure here
static void SemaphoreThread2(void const *argument)
{....for (;;)
{ if (semaphore != NULL) { /* Try to obtain the semaphore */ if (osSemaphoreWait(semaphore , 0) == osOK)If I use
if (osSemaphoreWait(semaphore , osWaitForever) == osOK) instead,It works fine!
Could anyone tell me why if (osSemaphoreWait(semaphore , 0) == osOK) works wrong?
#um1722 #freertos-stm32cubeSolved! Go to Solution.
2017-06-24 2:40 PM
I find the answer, It is because I am using the trace tool,they interact with each other
2017-06-24 2:40 PM
I find the answer, It is because I am using the trace tool,they interact with each other
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.