2016-09-20 10:00 AM
Hello everyone,
A week's search didn't bring me very far, so I thought I should ask You guys. I have some experience using Arduino, but this is my first hard-core microcontroller project and so far the learning curve has been insane.Anyway, I am using a stm32f4-discovery board, as an IDE I use Eclipse with the help of the HAL library. TIM3 is set up for base interrupts every 500ms for blinking two of the LEDs. I now want to set up TIM2 with the same type handle as TIM3 and attach an input capture on Channel 1 (PA0). I have connected PA0 and one of the LED pins. The goal is to get a counter value, which should be equivalent to 500ms. The problem is that I never enter the input capture interrupt. Can anyone tell me what is wrong with the code? See below:&sharpinclude <stdio.h>&sharpinclude <stdlib.h>&sharpinclude ''diag/Trace.h''&sharpinclude <stm32f4xx_hal.h>TIM_HandleTypeDef htim3;TIM_HandleTypeDef htim2;volatile uint32_t prev_time;volatile uint32_t pulse_length;volatile uint32_t count;void InitializeLED(){ __GPIOD_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = GPIO_PIN_12|GPIO_PIN_14; GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; GPIO_InitStructure.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);}void InitializeTimer3(){ __TIM3_CLK_ENABLE(); htim3.Instance = TIM3; htim3.Init.Prescaler = 48000; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 499; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim3.Init.RepetitionCounter = 0; HAL_TIM_Base_Init(&htim3); HAL_TIM_Base_Start_IT(&htim3); HAL_NVIC_SetPriority(TIM3_IRQn, 1, 0); HAL_NVIC_EnableIRQ(TIM3_IRQn);}void InitializeTimer2(){ __HAL_RCC_GPIOA_CLK_ENABLE(); __TIM2_CLK_ENABLE(); TIM_IC_InitTypeDef sConfigIC; htim2.Instance = TIM2; htim2.Init.Prescaler = 48000; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 65535; htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_BOTHEDGE; sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI; sConfigIC.ICPrescaler = TIM_ICPSC_DIV1; sConfigIC.ICFilter = 0; HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1); HAL_TIM_IC_Init(&htim2); HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1); HAL_NVIC_SetPriority(TIM2_IRQn, 2, 0); HAL_NVIC_EnableIRQ(TIM2_IRQn);}extern ''C'' void TIM3_IRQHandler(){ HAL_TIM_IRQHandler(&htim3);}extern ''C'' void TIM2_IRQHandler(){ HAL_TIM_IRQHandler(&htim2);}void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12|GPIO_PIN_14);}void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ pulse_length = __HAL_TIM_GetCompare(&htim2, TIM_CHANNEL_1); //read TIM2 channel 1 capture value __HAL_TIM_SetCounter(&htim2, 0); //reset counter after input capture interrupt occurs}void main(){ InitializeLED(); InitializeTimer3(); InitializeTimer2(); while(1) { count = __HAL_TIM_GetCounter(&htim2); }} #hal-library #input-capture2016-09-21 4:52 AM
Hi BesenSelqnin,
Yu should configure the TIM2_CH1 PA0 as well . ( put alternate function AF1). I think also that the line inside the main while loop is useless since you wil calculate the signal inside the callback. I recommend that you check the ready-to-use example inside the called ''TIM_InputCapture'' similar to you r case, at this path : STM32Cube_FW_F4_V1.13.0\Projects\STM324xG_EVAL\Examples\TIM\TIM_InputCapture -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.