2019-11-27 3:56 PM
I have troubles writing succesfully to flash on a STM32G07 chip.
The application is similar to this:
uint64_t data;
HAL_FLASH_Unlock();
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, addr, data);
HAL_FLASH_Lock();
I started getting hardfault in lock because of error in programming. I found out that this was related to timeout on the wait for operation to finish inside program function. So I added a check that program returning HAL_OK before calling lock . But this just moved the problem.
The behavious is very strange.
I can see that PGAERR and PGSERR in the FLASH SR register are being set.
My data is aligned at a 64-bit boundry I have added check that both data and the address i program to will have addr & 0x07 == 0.
I suspect some other interrupt could interefere in some way. But adding __disable_irq(); does not help.
Data is programmed like 25-50% of the times rest I simply get no data programmed.
2022-02-15 10:20 PM
Hello,
Could you solve your problem ? I have a exactly same problem right now, even IWDG is not enabled.
2023-02-19 10:53 AM
I could get HAL_FLASH_Program to write WORDS, as soon as I moved to doublewords the last error returned is PGA | PGS flags in the SR.
PGA = alignment
PGS = sequence
AFAIK, I have done everything correctly. There seems to be a problem with trying to write to FLASH on a 32f411RE. Worked hard to figure it out, I think there is something wrong with the libary, or at least how I am using it. Here is my code:
// STM32F411RE try to write doubleword into FLASH
// The flashing works for WORDS but not DOUBLEWORDS
#define SECTOR 7
#define ADDRESS 0x08060000
uint32_t lastError = 0;
uint64_t valueToWrite = ~0ULL;
uint64_t valueToRead = 0;
HAL_StatusTypeDef status = HAL_ERROR;
valueToRead = * ( uint64_t * ) ADDRESS;
if ( valueToRead == ~0ULL )
{
FLASH_EraseInitTypeDef pEraseInit = { 0 };
pEraseInit.TypeErase = TYPEERASE_SECTORS;
pEraseInit.Sector = FLASH_SECTOR_7;
pEraseInit.NbSectors = 1;
pEraseInit.VoltageRange = FLASH_VOLTAGE_RANGE_3;
uint32_t SectorError = 0;
do
{
HAL_FLASH_Unlock();
status = HAL_FLASHEx_Erase(&pEraseInit, &SectorError);
HAL_FLASH_Lock();
valueToRead = * ( uint64_t * ) ADDRESS;
} while( (status !=HAL_OK) || (SectorError != ~0UL ) || ( valueToRead != ~0ULL ) );
HAL_FLASH_Unlock();
status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, ADDRESS, valueToWrite );
HAL_FLASH_Lock();
lastError = 0;
if ( status != HAL_OK )
{
lastError = HAL_FLASH_GetError();
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.