2018-10-24 2:08 AM
Hi
On my board the ETH_DMABMR_SR bit never goes to zero and then exits for TIMEOUT.
Where did I make the mistake?
What exactly should I check?
Best Regards
Albert
2018-10-24 3:39 AM
Hello @infoinfo983 ,
In order to more understand the issue you are facing, we need more details on the case:
Which Hardware board used?
Are you using MII or RMII ? Is MII/RMII clock available from external source?
Do you have configured correctly the pins and enabled the clocks in RCC?
Kind Regards
Imen
2018-10-24 5:32 AM
Hi
The project was created with STM32cubeMX 4.27.0 and STlib 1.21.0. ... does not work. The microcontroller is STM32F429ZIT6. The interface is RMII. The ETH_REF_CLK is 50Mhz.
I tried to introduce a very old LwIP and oddly it works. In any case, I had to enter the following line of code in the HAL_ETH_Init (..) function on line 384
phyreg = heth-> Instance-> MACMIIAR; // FIXME
I'm looking for differences to understand where the problem is
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.