2018-12-11 6:46 AM
Hello all
I am new in this forum
And would like to get yours help regurding adding to my working code the TCP to Modubs RTU client protocol.
the code is working on STM32F103 and I intend to add to my PCB Ethernet TCP to Serial RS232 Module in order to enable Ethernet link.
can anyone send information that can help me to understand if possible to start with this kind of code modification
thanks
Ilan
2018-12-11 10:26 PM
> ... adding to my working code the TCP to Modubs RTU client protocol.
I hope you don't overreach.
There is no "Modbus TCP to RTU" protocol. RTU and TCP are variants of the same protocol over different media. Your product would be a gateway.
And having worked with both, don't understimate it. Both media (serial & Ethernet) have quite different properties, and are not trivial to handle (if you want a robust product).
The first step would be do download the protocol specifications, and study them carefully.
2018-12-12 6:54 AM
Hi
and thanks for your response
I think I did mistake here, I need to implement Modbus TCP
Server (my device is a slave)
And I intend to add to my PCB Ethernet TCP to Serial RS232
Module in order to keep using ST F series
do you think /know if it will be difficult to handle this kind
of hardware configuration will prevent to achieve robust product
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.