2025-04-05 6:21 AM
Hi,
I am running a simple TCP server using the lwIP stack and no RTOS. I got help from the "Echo_Server" example offered in most ST eval board packages, everything works fine.
I need to accept a single socket connection from the outside and maybe also establish one as a client.
I understand that because sockets are sort of blocking, they are often implemented in a multi-thread environment. I am trying to not use any OS. Any type of the F series microC will do.
Has anyone ever implemeted lwIP sockets without any OS? Can it be done?
Thank you.
2025-04-05 7:30 PM
We know the API as it is requires those mechanisms and therefore some sort of OS. That has been stated a thousand times already in this thread. The question is: has someone done it without an OS (cherry on top would be to know how).
2025-04-05 11:14 PM
With blocking code, everything that needs to be done to unblock must happen “by magic” - in other threads or by interrupt service routines. And things like semaphores, thrrad-safe queues are all helpful.
An OS will provide calls for those.
Or you could write them from scratch.
I use the “Crossworks Tasking library” that comes with the (paid-for) Rowley Crossworks IDE to give me multiple threads, semaphores etc. I don’t regard it as an Operating System. Does that count as an OS or not by your criteria?
A lot of my decisions are historic - the project started pre-stm32cube. And I like the Rowley Crossworks IDE.
I use the netconn api of LWIP. Do you specifically want their Socket API?
I suppose I should add that my system can accept incoming TCP connections.
So whether or not I have succeeded depends on your specific interpretation of terms like socket an OS
2025-04-07 6:30 AM
Interesting.. Thanks for sharing.
@Danish1 wrote:I use the “Crossworks Tasking library” that comes with the (paid-for) Rowley Crossworks IDE to give me multiple threads, semaphores etc. I don’t regard it as an Operating System. Does that count as an OS or not by your criteria?
The owners themselves call it an RTOS, so I guess it does count as an OS. From Rowley's website: "CTL is a real-time operating system designed for deployment in embedded systems that require a solid foundation to support their application infrastructure.".
@Danish1 wrote:So whether or not I have succeeded depends on your specific interpretation of terms like socket an OS
Forgive me but there isn't any "interpretation of terms" on my end. A TCP socket is a TCP socket. lwIP's Netconn is a broader TCP API and their Socket API relies on it, sure, but it is not socket.
Your work was definitely in the same realm as the question I asked, but it was not baremetal and it was not socket.
2025-04-22 8:31 AM
I don't know if it's late or not but here is a code i used for a baremal tcp server that handles client (only one but just extend the client to a list)
You just have to configure the .ioc to work as a tcp server lwip, straightforward.
I also have a websocket implementation baremetal if needed.
also reach my email if any more question (i don't get any notifications here):
leo.fresnay@apyretechs.com
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.