2017-07-18 11:26 AM
Hello
I have made a few projects using the CubeMX that include LwIP. Each time I had compiler errors concerning MEMP_ defines which are marco-generated. If I would use any feature that require the use of one of these defines ex: when creating a pcb, The compiler gives me an error saying that the define cannot be resolved.The solution to this problem is to add : &sharpinclude 'lwip/memp.h' to my main.c. Which is weird because memp.h is sub included in lwip.h file (which s included in main.c).Also when deleting the error message from the list and re-building the project the compiler doesn't always trigg an error message.Could this be an error witht he macro itself , a bug in CubeMX when creating the project or a missinterpretation of the precompiler ?Even tho I fixed the error im still curious about what is causing this.I'm sure one of you precompiler and makefile wizzards could bring up possible causes.I am using discoveryF4 board with most recent version of CubeMX and SW4STM32. -Andy#lwipWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.