2025-07-28 2:02 AM
Hello everyone,
in my current project, I'm working with a Nucleo H743ZI2 (with an STMH743ZIT6). My goal is to read audio data from MEMS microphones using DMA and DFSDM filters. The ultimate aim is to build an 8-microphone array, but for the first step, I only want to read data from a single microphone. And this is exactly where my problem lies: currently, no data is being saved in RAM. I suspect the problem is with DMA, as I've observed the following:
DFSDM:
DMA:
It seems to me that DMA is not starting correctly or that something in the configuration is incorrect. Even when I try to start the DMA manually by the following function, no interrupt is triggered:
void start_DMA1_Stream0(void)
{
DMA1_Stream0->CR = 0;
while (DMA1_Stream0->CR & DMA_SxCR_EN);
DMA1_Stream0->PAR = (uint32_t)DFSDM1_FLT0_CR1; // Peripherie adress
DMA1_Stream0->M0AR = (uint32_t)&audioBuffer; // buffer where the data shoul be stored
DMA1_Stream0->NDTR = 1024; // Sample count
DMAMUX1_Channel0->CCR = 101;
DMA1_Stream0->CR = (1 << 2) | // Transfer error interrupt enable
(1 << 3) | // Half transfer interrupt enable
(1 << 4) | // Transfer complete interrupt enable
(1 << 8) | // Circular Mode
(1 << 10) | // Memory increment
(1 << 12) | // Peripheral data size = word
(1 << 14) | // Memory data size = word
(1 << 0); // Enable
}
I have attached main.c below, maybe someone can help me with my problem. It also contains a few debugging functions that are not so important.
Thank you in advance.
Solved! Go to Solution.
2025-07-29 2:05 AM - edited 2025-07-29 2:08 AM
Hi @Saket_Om
Thanks for your reply but I solved it 2 hours ago :)
For the solution I had a look at these two posts:
https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/ta-p/49498 https://en.eeworld.com.cn/mp/STM32/a60611.jspx
I found that the actual problem was related to memory access: the buffer I used for the audio data (audioBuffer) was placed in DTCM RAM (starting at address 0x20000000) by default. However, DMA1 on the STM32H7 series cannot access DTCM. According to the reference manual (RM0433), DMA1 and DMA2 can only access specific RAM regions like AXI-SRAM, SRAM1-3 (D2 domain), and SRAM4 (D3 domain).
To solve the problem, I explicitly placed the buffer into RAM_D2, which is accessible by DMA1:
/* Section for variables that must reside in RAM_D2 (for DMA) */
/* All variables marked with __attribute__((section(".RamD2"))) go here */
.RAM_D2 (NOLOAD) :
{
. = ALIGN(4);
*(.RamD2)
. = ALIGN(4);
} >RAM_D2__attribute__((section(".RamD2"))) int32_t audioBuffer[AUDIO_BUFFER_SIZE];After this change, the DMA transfer started working immediately — data is now written into the buffer, and the DMA complete callback is triggered as expected.
2025-07-29 1:37 AM
Hello @MannyMarc35
Could you please share your files hal_msp.c and it.c then we can assist you more effectively.
2025-07-29 2:05 AM - edited 2025-07-29 2:08 AM
Hi @Saket_Om
Thanks for your reply but I solved it 2 hours ago :)
For the solution I had a look at these two posts:
https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/ta-p/49498 https://en.eeworld.com.cn/mp/STM32/a60611.jspx
I found that the actual problem was related to memory access: the buffer I used for the audio data (audioBuffer) was placed in DTCM RAM (starting at address 0x20000000) by default. However, DMA1 on the STM32H7 series cannot access DTCM. According to the reference manual (RM0433), DMA1 and DMA2 can only access specific RAM regions like AXI-SRAM, SRAM1-3 (D2 domain), and SRAM4 (D3 domain).
To solve the problem, I explicitly placed the buffer into RAM_D2, which is accessible by DMA1:
/* Section for variables that must reside in RAM_D2 (for DMA) */
/* All variables marked with __attribute__((section(".RamD2"))) go here */
.RAM_D2 (NOLOAD) :
{
. = ALIGN(4);
*(.RamD2)
. = ALIGN(4);
} >RAM_D2__attribute__((section(".RamD2"))) int32_t audioBuffer[AUDIO_BUFFER_SIZE];After this change, the DMA transfer started working immediately — data is now written into the buffer, and the DMA complete callback is triggered as expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.