STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Touch Sensing issue with ChD->Delta

Greetings! I am testing a touch button in a custom board using stm32u585 mcu. I try to follow the following workshops available on YouTube: Workshop 1 Workshop 2 The thing is, I tested in Debug Mode like in Workshop 1 in minute 15 and I could see the...

Resolved! USART busy just after initialization

Hello,Working on STM32F767BITx and using Free RTOSEnable USART2, here is the init codestatic void MX_USART2_UART_Init(void) { huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.St...

STM32F746 LWIP + FreeRTOS CMSIS V2

Hi,I'm using an STM32F746G-DISCO board and I'm just trying to build a build a simple project with LWIP and FreeRTOS using CMSIS V2 however after enabling the minimum hardware using CubeMX I am unable to get any ping replies from the board. If I use C...

marcinq by Associate
  • 3433 Views
  • 6 replies
  • 2 kudos

USBX CDC ACM Write problem

Hello everyone,I'm developing an application using USBX CDC ACM class in standalone mode. I've written an execution loop for scheduling USB stack operations and there are no problem with READ transaction; i'm able to receive correctly every data from...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.