2019-11-14 12:10 PM
Hi. I noticed in the latest STMCubeIDE v1.1.0 DMA is initialized at the end of initialization chain. There is only NVIC interrupt priority set but as i can see it's important where it's initialized.
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_DMA_Init();
instead of previous
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
The result is while UART IDLE interrupt occurs, DMA shows me always that is received 0 bytes in NDTR register.
my code(working with correct initialization order): https://github.com/lamik/UART_DMA_receiving
2019-11-17 10:44 PM
Having the same problem, generating code for a STM32F100VETx while using ADC1 and DMA. DMA is initialized after ADC1 which does not work if DMA is used to query the ADC. Switching the initialization order resolves the problem.
2019-11-19 11:38 PM
Same problem appears on CubeMX5.4.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.