STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lwIP TCP STM32F7

I'm developing an ethernet application on a NUCLEO-F746ZG board using the LWIP library. My app basically consists of the board (ip:192.168.1.21) is receiving a message every 20ms form a TCP client (my PC ip: 192.168.1.150) while the board sends UDP m...

0690X000008i5uZQAQ.png

USB composite CDC + DFU

I would like to use DFU and CDC composite USB devices on STM32L433.Implemented USB descriptors to support DFU and CDC.However DFU was not enumerated properly.Looks like this is USB driver issue.Depending on PID,DFU is enumerated or not.i.e.In case PI...

YChun.15 by Associate
  • 1070 Views
  • 0 replies
  • 1 kudos

Add FreeRTOS to Discovery Node IoT Kit

Has anyone added FreeRTOS to the discovery node iot kit?I've ported freertos several times before (and have donei t on the Nucleo f411) without issue...but it is getting hung up as I try to get it set up with the discovery kit.I am setting the sys ti...

DSabo by Associate III
  • 907 Views
  • 1 replies
  • 0 kudos

SPI bootloader fails to accept every other command.

I am trying to use the SPI bootloader on a Nucleo F446ZE board and have problems when issuing commands. The symptom is that every other command is not acknowledge and every other works fine. Trying for instance the GET_VERSION command gives the follo...

THamb by Associate II
  • 4175 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.