2025-02-04 5:31 AM
I'm using STM3G0B1 as I2C SLAVE device with NVIC+NoStretchMode since I2C Master device doesn't support the clock stretching.
When HAL_I2C_AddrCallback is called (Read request from Master device), HAL_I2C_Slave_Seq_Transmit_IT seems not working because 0xFF is transmitted, not the expected value held by I2C_REGISTERS.
I guess 0xFF is the default value with NoStretchMode to respond immediately to the request.
How to resolve this issue? Is there a way to transmit the correct data with NoStretchMode for Read request?
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
...
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode) {
if (TransferDirection == I2C_DIRECTION_TRANSMIT) {
if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, ®Addr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Receive Data", __func__, __LINE__);
return;
}
} else {
if (HAL_I2C_Slave_Seq_Transmit_IT(hi2c, I2C_REGISTERS + regAddr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Transmit Data", __func__, __LINE__);
return;
}
}
}
Solved! Go to Solution.
2025-02-13 4:56 PM
I was able to resolve this by presetting the value to TXDR in HAL_I2C_SlaveRxCpltCallback.
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c) {
hi2c->Instance->TXDR = regAddr;
}
2025-02-04 7:30 AM
Hello @ShoH
You are setting a receive process when "TransferDirection == I2C_DIRECTION_TRANSMIT".
Please try with the snippet code below:
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
...
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode) {
if (TransferDirection != I2C_DIRECTION_TRANSMIT) {
if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, ®Addr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Receive Data", __func__, __LINE__);
return;
}
} else {
if (HAL_I2C_Slave_Seq_Transmit_IT(hi2c, I2C_REGISTERS + regAddr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Transmit Data", __func__, __LINE__);
return;
}
}
}
2025-02-04 5:45 PM
Hi @Saket_Om, thank you for your reply.
The condition for direction seems to be correct as “TransferDirection == I2C_DIRECTION_TRANSMIT”.
(I tried “TransferDirection != I2C_DIRECTION_TRANSMIT”, the I2C transaction was corrupted and MCU rebooted.)
When tramsmitting Write Request (Data=Register Address) then Read Request from Master device, HAL_I2C_Slave_Seq_Receive_IT is called correctly to receive Register Address, and then HAL_I2C_Slave_Seq_Transmit_IT is called. However, because Clock Stretching is disabled, it seems that 0xFF is transmitted immediately before that and HAL_I2C_Slave_Seq_Transmit_IT is ignored.
If I preset "hi2c->Instance->TXDR = 0x5a" after HAL_I2C_Slave_Seq_Receive_IT as follows, 0x5a is transmitted in response to Read Request instead of 0xFF.
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
...
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode) {
if (TransferDirection == I2C_DIRECTION_TRANSMIT) {
if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, ®Addr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Receive Data", __func__, __LINE__);
return;
}
hi2c->Instance->TXDR = 0x5a;
} else {
if (HAL_I2C_Slave_Seq_Transmit_IT(hi2c, I2C_REGISTERS + regAddr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Transmit Data", __func__, __LINE__);
return;
}
}
}I have attached the relevant source codes. It would be helpful if you give an additional advice.
2025-02-13 4:56 PM
I was able to resolve this by presetting the value to TXDR in HAL_I2C_SlaveRxCpltCallback.
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c) {
hi2c->Instance->TXDR = regAddr;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.