2026-04-20 8:38 PM - edited 2026-04-20 11:25 PM
I am coding from the scratch to learn how STM32 works with MIPI-DSI LCD, because I am going to use customized MIPI-DSI LCD. I refer to the official code, but some incorrect content as below:
official default code: in main.c , static void MX_LTDC_Init(void):
// SETVCOM
uint8_t InitParam60[4] = {00, 00, 00, 0xC0};
if (HAL_DSI_LongWrite(&hdsi, 0, DSI_DCS_LONG_PKT_WRITE, 4, 0xC7, InitParam60) != HAL_OK)
{
Error_Handler();
}
BUT, I check HX8379C datasheet (LCD control ), SETVCOM command is (B6h), and there is no 0xC7 command ?
so what's this code for? and HX8379C datasheet dosen't mention initial sequence , how do we know that we need to set SETPOWER, SETDISP, Set display cycle timing,.....SET GAMMA,....,then Exit Sleep Mode to let LCD work?
I don't use touchgfx now, just want to test if DSIHOST, LTDC work successfully, so I declare a framebuffer[480*480] then in MX_LTDC_Init(), write:
pLayerCfg.FBStartAdress = (uint32_t)framebuffer;
then using for loop to fill it red, but the screen is still black
2026-04-22 8:12 AM
Hello @emmaulala
@emmaulala wrote:
I refer to the official code, but some incorrect content as below:
Could you please specify the name of the example you are referring to?
2026-04-22 6:07 PM - edited 2026-04-22 7:36 PM
These 2 examples contains what I mentioned incorrect: the example from touchGFX Designer of STM32U5A9J-DK, in main.c , in function MX_LTDC_Init, and the example from firmware package (\Repository\STM32Cube_FW_U5_V1.8.0\Projects\STM32U5x9J-DK\Examples\DSI\DSI_VideoMode_SingleBuffer), in main.c, in function SetPanelConfig, what's 0xC7 cmd for?
BTW, I refer to VideoMode_SingleBuffer example, and I succeed in displaying on the screen, and now I turn on ThreadX and touchGFX, and follow the instruction (https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-dsi-video-mode), and I keep singlebuffer location 0x200D0000 with touchgfx, after turning on LTDC interrupt, I succeeded!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.