2024-04-02 1:04 AM - last edited on 2024-06-10 6:27 AM by Amel NASRI
I want to send audio samples (received via SAI1 from PDM MIC) to SAI2_SD_B as SPDIF out.
It does not work, because: the DMA does not seem to write the DR in SAI2:
Remark: it is on a STM32U5A5RJT6Q (LQFP64 package): the datasheet "says": not a SAI2 there (just one SAI) - but not true - it works also with SAI2, even CubeMX does not let me configure SAI2 pins (also wrong in CubeMX tool). But I can configure SAI2 and see it working (in Polling and INT mode, just the DMA fails).
So, my impression: the circular buffer and DMA does not work. No idea why not: the code is generated by CubeMX.
This topic is related to this thread:
Solved: STM32U5xx: SPDIF out - how to configure? - STMicroelectronics Community
Here is the DMA config I use: Why does it send all as zero (or does not send anything into SAI2_B DR)?
/* Peripheral DMA init - SAI2_SD_B as SPDIF - use CH5 */
NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
NodeConfig.Init.Request = GPDMA1_REQUEST_SAI2_B;
NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
NodeConfig.Init.Direction = DMA_MEMORY_TO_PERIPH;
NodeConfig.Init.SrcInc = DMA_SINC_INCREMENTED;
NodeConfig.Init.DestInc = DMA_DINC_FIXED;
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
NodeConfig.Init.DestDataWidth = DMA_SRC_DATAWIDTH_WORD;
NodeConfig.Init.SrcBurstLength = 1;
NodeConfig.Init.DestBurstLength = 1;
NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
NodeConfig.Init.Mode = DMA_NORMAL;
NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel5) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel5, NULL, &Node_GPDMA1_Channel5) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel5) != HAL_OK)
{
Error_Handler();
}
handle_GPDMA1_Channel5.Instance = GPDMA1_Channel5;
handle_GPDMA1_Channel5.InitLinkedList.Priority = DMA_LOW_PRIORITY_MID_WEIGHT;
handle_GPDMA1_Channel5.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel5.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
handle_GPDMA1_Channel5.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel5.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel5) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel5, &List_GPDMA1_Channel5) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hsai, hdmatx, handle_GPDMA1_Channel5);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel5, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
BTW: what is "DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0"?
It is the same for the SAI1 DMA, using channel 4, with quite similar config (just direction is reversed), but also PORT0 used there. Is this a conflict? (even the channel is a different one).
Why is the circular DMA buffer config not working for Memory-to-SAI2_B?
Solved! Go to Solution.
2024-07-10 6:27 PM
close the ticket
2024-07-10 6:27 PM
close the ticket
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.