2024-07-02 1:26 AM
The ADC seem to work when i run this code.
Internal ADC like vref vbat and internal temperature seem to be working and I testes it with cold spay and checked the internal temperature.
the ADC input pins seem to be stuck ate a level and not change or giving the write value
ADC::ADC()
{
if (ADC_BUF_LEN != hadc1.Init.NbrOfConversion) {
Error_Handler();
}
HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED);
this->rcvd = true;
if (HAL_ADC_Start_DMA(&hadc1, (uint32_t *) adc1_buf, ADC_BUF_LEN ) != HAL_OK) {
/* Start Error */
Error_Handler();
}
}
ADC::~ADC()
{
}
ADC *ADC::getInstance()
{
static ADC adc = ADC();
return &adc;
}
void ADC::rcvdData()
{
this->rcvd = true;
}
bool ADC::getNumValue(uint32_t *value, adc_input_t idx)
{
switch (idx) {
case ADC1_IN1_MCU_ADC_VMON_3V3 :
case ADC1_IN2_MCU_ADC_VMON_5V0 :
case ADC1_IN3_MCU_UVOV_IMON :
case ADC1_IN5_DAC_PTR_POWER :
case ADC1_IN6_ESC_POINTER_I_MON :
case ADC1_IN8_MCU_UVOV_IMON :
case ADC1_IN9_MCU_ADC_VMON_15V0 :
case ADC1_IN10_ASSEMBLY_ID :
*value = __HAL_ADC_CALC_DATA_TO_VOLTAGE(&hadc1, adc1_buf[idx], 2500, hadc1.Init.Resolution);
return true;
break;
case ADC1_VREF :
*value = __HAL_ADC_CALC_VREFANALOG_VOLTAGE(&hadc1, adc1_buf[idx], hadc1.Init.Resolution);
return true;
break;
case ADC1_VBAT :
*value = __HAL_ADC_CALC_DATA_TO_VOLTAGE(&hadc1, adc1_buf[idx], 2500, hadc1.Init.Resolution) * 4;
return true;
break;
case ADC1_TEMP :
*value = __HAL_ADC_CALC_TEMPERATURE(&hadc1, adc1_buf[idx], 2500, hadc1.Init.Resolution) * 1000;
return true;
break;
default:
return false;
}
}
void ADC::update()
{
if (this->rcvd) {
}
}
void HAL_ADC_ErrorCallback(ADC_HandleTypeDef *hadc)
{
Error_Handler();
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
if (hadc->Instance == ADC1) {
}
}
t
2024-07-02 7:31 AM
Hello @JulioAndrade ,
Please specify the STM32 product you are using, and could you please provide more details on your configuration project, If possible, please attach your .ioc file or a ZIP of the project? This would help us to reproduce the issue and find a solution.
2024-07-03 1:46 AM
2024-07-09 12:55 AM
hello are you guys still looking at this ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.