STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Failed to start GDB(RCC?STM32CUBEIDE update error?)

Hola,Desde hace unos días me encuentro con el siguiente error en un programa que había completado. Lo único que hice ese día fue cambiar el tiempo de retraso; No cambié nada más.[Imagen: Foto 1]Después de horas de búsqueda, encontré en el foro que bo...

System freezes, stuck in USART interrupt

The MCU is STM32F469, using RTOS: AZURE ThreadX and FatFS. The system is fetching data through 3 UART ports and doing logging (saving data into a file).Logging is setup to run once one hour, about 1000 bytes.UART read and write both use DMA. The syst...

jason_gu by Associate
  • 3408 Views
  • 3 replies
  • 1 kudos

USB HID Keyboard LEDs

Posted on June 13, 2014 at 07:33 Finally find the way out of the Keyboard LEDs working. I use STM32F4 disc with STM32Cube_FW_F4_V1.1.0 and STM32CubeMX 4.2 The HID keyboard program is modified from HID Mouse program Update the usbd...

zg by Associate
  • 3544 Views
  • 2 replies
  • 2 kudos

Resolved! I2C Slave Wrong Read Count (NUCLEO-U5A5ZJ-Q)

Hey there :)I am having trouble running the nucleo (NUCLEO-U5A5ZJ-Q) as an I2C slave where read/write sizes are unknown (only known by master)For the configuration I am using CubeMX and most of the time the slave is working quite fine. However someti...

PWM frequency is not as expected

Hi,I'd like help to understand what is thew PWM frequency.As far as I understand:1. The main system clock is 64MHZ -- see below SystemClock_Config()2. PWM frequency is 64KHz (= 64MHZ / (1000 - 1))BUT, measuring the frequency shows 4KHz (rather than 6...

AFink by Associate III
  • 1647 Views
  • 2 replies
  • 0 kudos

Resolved! How to count how many files exist in the SD card

Hy guys, I want to be able to create a named file in an SD card based on how many files I have in the directory, per example: if I have only 1 file "file1", I'll create the next one as "file2". I searched the ff.h library, but didn't find anything th...

FPicc.1 by Senior
  • 5508 Views
  • 9 replies
  • 1 kudos

Resolved! STM32H7 Firmware Update Using Web Server

Hi all,AbstractWe are developing our product based on STM32H7. We would like to use the HTTP server and Netconn to update the firmware for our product. We consider this method easy to use for customers more than Serial or USB. We have tried looking f...

HHuyn.4 by Associate III
  • 2648 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.