2023-04-19 5:19 PM
I am using the UX_Host_MSC example project. When a connect a USB drive to the USB-C port, the demo app detects a physical connection but power is never activated.
Solved! Go to Solution.
2023-04-20 3:36 PM
Thanks JW. The project is designed to support the TCPP03. I discovered my mistake in re-reading the "ReadMe" file. JP25 (power control block) is NOT mutually exclusive. It required both the power source (5V_EXT for example) AND 5V_UCPD in order to source USB power. I had originally assumed JP25 only specified the main power provider.
--KB
2023-04-20 2:07 AM
According to schematics and UM2854, UCPD (USB-C Power Delivery) is handled by a dedicated chip, TCPP03. Is that chip handled in the example project you've mentioned? If not, isn't there a dedicated example project for UCPD?
JW
2023-04-20 3:36 PM
Thanks JW. The project is designed to support the TCPP03. I discovered my mistake in re-reading the "ReadMe" file. JP25 (power control block) is NOT mutually exclusive. It required both the power source (5V_EXT for example) AND 5V_UCPD in order to source USB power. I had originally assumed JP25 only specified the main power provider.
--KB
2023-04-20 11:49 PM
Ah. That board is complex indeed, even in the basics i.e. power supplies.
Thanks for coming back with the solution. Please select you post a Best do that the thread is marked as solved.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.