2024-08-30 4:24 AM - last edited on 2024-08-30 4:34 AM by mƎALLEm
I'm using STM32CubeMX 6.12.0, with the firmware package U0_V1.1.0.
When generating code for a STM32U073, the file system_stm32u0xx.c is generated, which contains the implementation of the SystemCoreClockUpdate() function.
This file seems to be a mere copy of the firmware package's file "<...>\STM32Cube\Repository\STM32Cube_FW_U0_V1.1.0\Drivers\CMSIS\Device\ST\STM32U0xx\Source\Templates\system_stm32u0xx.c"
I'm attaching it for reference.
On line 330 we have:
tmp = AHBPrescTable[((RCC->CFGR & RCC_CFGR_HPRE) >> 4U) & 0xFU];
It seems that this should actually be
tmp = AHBPrescTable[((RCC->CFGR & RCC_CFGR_HPRE) >> RCC_CFGR_HPRE_Pos) & 0xFU];
since RCC_CFGR_HPRE_Pos is 8, not 4 (as defined in stm32u073xx.h:5524).
The RM agrees with the value 8: §5.4.3 shows HPRE[3:0] in position [11:8] in RCC_CFGR.
Also note that stm32u0xx_hal_rcc.c:396 has the correct value (it uses the macro RCC_CFGR_HPRE_Pos, in HAL_RCC_OscConfig()).
Note also that the same bug potentially affects the system_stm32 file for every other MCU family too, since the shift amount is always hardcoded as 4 rather than use the macro, though other families might actually be fine with the value 4.
Solved! Go to Solution.
2025-06-30 7:28 AM
2024-08-30 4:28 AM
Hello @SZano
I'm analyzing it and get back to you as soon as possible.
2024-09-03 6:20 AM
Internal ticket number for follow up: 190058 (not accessible by the community users).
I will get back to you for any feedback.
2025-06-30 7:28 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.