2025-11-13 2:23 AM - last edited on 2025-11-18 2:19 AM by Amel NASRI
Hello
I have custom board with STM32N657. I have set timer 2 to output PWM pulse on channel3 and output compare pulse on channel 1 as trigger to another timer. The timer starts when external trigger - TIMER4_ETR (mapped to timer 2) detects rising edge. All works good, there are continuous pulses as expected.
I want timer2 to run once per trigger so enabling One Pulse Mode.
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = TIM2_PRESCALER;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = TIM2_PERIOD;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
// if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
// {
// Error_Handler();
// }
// if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
// {
// Error_Handler();
// }
if (HAL_TIM_OnePulse_Init(&htim2, TIM_OPMODE_SINGLE) != HAL_OK)
{
Error_Handler();
}
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_TRIGGER;
sSlaveConfig.InputTrigger = TIM_TS_ETRF;
sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;
sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;
sSlaveConfig.TriggerFilter = 0;
if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
HAL_TIMEx_RemapConfig(&htim2, TIM_TIM2_ETR_TIM4_ETR);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
sConfigOC.Pulse = TIM2_PULSE_CH1;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
__HAL_TIM_ENABLE_OCxPRELOAD(&htim2, TIM_CHANNEL_1);
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = TIM2_PULSE_CH3;
sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
TIM_CCxChannelCmd(htim2.Instance, TIM_CHANNEL_1, TIM_CCx_ENABLE);
TIM_CCxChannelCmd(htim2.Instance, TIM_CHANNEL_3, TIM_CCx_ENABLE);
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}
//Then in main
HAL_TIM_Base_Start_IT(&htim2);
The above code configures timer2 to OPM mode but no output pules are generated when triggered.
When clearing OPM bit, TIM2->CR1 &= ~TIM_CR1_OPM, and starting timer with external trigger then output channels generate pulses again so configuration seems to be correct in non-OPM mode.
Any suggestion where might be a problem?
Examples show how to configure OPM with TIxFPx trigger but non with external trigger.
2025-11-19 7:06 AM
Hello,
did you check that he following condition is met (refer to RN0486, section:50.3.22)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.