STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBX Host MSC Standalone functions missing

I am on an H562 and trying to rd/wr a file on a USB memory stick using the mass storage controller. I am trying to understand what to do about this block when I am running in standalone mode. I started from an example code which is in RTOS mode but I...

Capocc_1-1763462236696.png Capocc_2-1763462321952.png Capocc_3-1763462637638.png
Capocc by Associate II
  • 1026 Views
  • 6 replies
  • 1 kudos

Accurate timing of events - SPI DMA

In the above image (logic analyzer) , SPI in DMA was supposed to start at the end of high on the second signal, but it starts a bit later. (3rd signal CS of SPI, 4th signal SCLK)And the SPI was to supposed to be active at every period (the first sign...

sreyas40_0-1762943386543.png sreyas40_1-1762943518981.png sreyas40_2-1762943888502.png

Interupt is not processing the signal

Hi I am trying to migrate my code from SPL(old version) to HAL based code I have conveted the  same setup code to cubemx to generate the init function and I am using a clrc663 IC(card reader) along with it when the Ic Generates an interupt the mcu do...

naveen-0 by Associate II
  • 948 Views
  • 6 replies
  • 2 kudos

LPUART fail wakeup in STOP2

Hello, Using Modbus master and slave communication, where Modbus master working fine, I have issue with slave device communication. Using HAL_UARTEx_ReceiveToIdle_IT() for receiving modbus frame, and HAL_UART_Transmit_IT() to transmit response. Curre...

npatil15_0-1762921775853.png npatil15_1-1762921798795.png

ADC + DMA on STM32H753ZI

Hi All, I have a question regarding the validity of my implementation of ADC + DMA on the STM32H753ZI. I had quite a lot of trouble getting the HAL_ADC_ConvCpltCallback configured as void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) { coun...

eskilru by Associate
  • 666 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 Nucleo audio input using SAI with GPDMA

Hello everyone,I'm trying to configure the SAI and GPDMA peripherals on an STM32 to acquire audio from an I2S microphone. My goal is to capture a 32-bit, 2-channel audio stream at a 16 kHz sample rate, with the STM32 acting as the clock master. I've ...

jweber by Associate II
  • 2012 Views
  • 5 replies
  • 0 kudos

STM32C0 rewrite flash without erase

Hey all,I'm trying to get embedded Lua (https://eluaproject.net/) running on an STM32C0 MCU. The implementation has a Write Once Filesystem that uses flash and can be appended to but not modified.The issue is that the WOFS relies on being able to wri...

rous by Associate
  • 754 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.