2025-06-25 4:01 AM - edited 2025-06-25 4:02 AM
Hi,
Looking into STM32CubeN6\Projects\STM32N6570-DK\Examples\SD\SD_ReadWrite_DMA example,
I see that quite heavy operations are used:
SCB_CleanDCache_by_Addr (aTxBuffer, BUFFER_SIZE);
// ...
SCB_InvalidateDCache_by_Addr (aRxBuffer, BUFFER_SIZE);while the aRxBuffer[] and aTxBuffer[] are located in a noncacheable memory region.
uint8_t aTxBuffer[BUFFER_SIZE]__NON_CACHEABLE;
uint8_t aRxBuffer[BUFFER_SIZE ]__NON_CACHEABLE;Could you please explain why?
Regards,
A
Solved! Go to Solution.
2025-10-31 1:50 AM
2025-07-30 2:25 AM
Hello @ERROR
Thank you for bringing this issue to our attention.
I reported this internally.
Internal ticket number: 213510 (This is an internal tracking number and is not accessible or usable by customers).
2025-10-27 4:45 AM
2025-10-27 5:02 AM
Presumably for illustration of method for cache coherency.
Would depend on Linker Script and suitable memory region allocation and MPU configuration.
2025-10-27 5:23 AM
Hello @ERROR
The issue has been resolved internally by removing the __NON_CACHEABLE attribute from the buffer declarations, as shown below:
/******** SD Transmission Buffer definition *******/
uint8_t aTxBuffer[BUFFER_SIZE];
/**************************************************/
/******** SD Receive Buffer definition *******/
uint8_t aRxBuffer[BUFFER_SIZE];
/**************************************************/
The fix will be available on st.com in the next release.
2025-10-31 1:50 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.