2021-03-26 6:08 AM
Hello community,
I'm currently having issues or perhaps not fully understanding the procedure of writing data to the MCU bank 2 and then switching to this bank to run the program from bank 2.
My setup for now is using a custom protocol for sending the generated .bin file through uart. I am currently just sending the .bin file in chunks to the first addr of bank 2(0x08080000) and incrementing it for every 8 byte write.
I do erase the bank 2 before writing to it. Here my understanding is that the number of pages is 127 and i start on page 0.
Once the write is done my unnderstanding is I should enable the BFB2 bit inorder for the MCU to boot from BANK2 once the system resets?
I have not been able to switch successfully, because I still get returned bank 1 being used when BFB2 bit is set.
2021-04-02 3:39 AM
Use GO command to tell the application code start address.
If you could share your UART communication code block , It would be helpful to me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.