2016-04-12 7:20 PM
Hi folks,
I am a little confused about USB termination requirements on the STM32L476 part. I read in the datasheet that termination resistors on D+/D- are not needed and that the impedance matching is done by the internal PHY (as well as pull-up).However, I was reviewing the schematics for the STM32L4 Discovery board and it shows that termination resistors are used externally. As I would consider this a reference design, I am a bit confused by the discrepancy.Are the 22 Ohm termination resistors needed on D+/D- with this part or not?Thanks,RobPS -- This forum software is absolutely horrible. It is impossible to tell if this question has already been asked and answered. #usb #stm32l4-discovery-usb2016-04-13 6:04 AM
Hi Rob,
As it is mention in the STM32L476 related datasheet: no external termination series resistors are required on USB_DP (D+) and USB_DM (D-); the matching impedance is already included in the embedded driver.Regarding the discovery schematic, the issue has been reported internally -Syrine-2016-04-13 6:18 AM
> I am a little confused about USB termination requirements on the STM32L476 part.
> Are the 22 Ohm termination resistors needed on D+/D- with this part or not? Any external series resistors are not required on D+/D- lines. In STM32L476xx datasheet (
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00108832.pdf
), ''Table 89. USB electrical characteristics'' (p190) section, you'll see this note:3. No external termination series resistors are required on USB_DP (D+) and USB_DM (D-);the matching impedance is already included in the embedded driver. For more confirmation, the driver impedance value on this table, ZDRV (Output driver impedance): 28(min), 44(max) Ohm is apparently aware of this requirement on the USB 2.0 spec,7.1.1.1 Full-speed (12 Mb/s) Driver Characteristics (usb20_pdf)the impedance of each of the drivers (ZDRV) must be between 28 Ohm and 44 Ohm That is, any external resistor is supposed in the output driver design. Tsuneo PS. Ah, while I'm writing my answer, the question has been answered.. Sorry for duplicated answer.
2016-09-29 5:30 AM
That answer really helps me cause i encountered some bad risetime in my new configuration.
However we use both FS and HS port but i cant find any about this in the HS section. Is the termination internal only for the FS.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.