STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL callback's got me curios

Posted on August 17, 2016 at 09:42 Hi guys, I am currently working on an library myself, and I like the way st is doing certain things, so I am ''lending'' myself ideas from the HAL. One thing in particular caught my eye, the callb...

hof2 by Associate II
  • 1093 Views
  • 1 replies
  • 0 kudos

DMA of STM32F4 questions about some parameters

Posted on August 17, 2016 at 17:35Hello,     i am trying to program DMA of STM32F4-DISCOVERY board. But I am not able to understand some parameters. 1.In Burst mode, what does  an incremental burst transfer of 4/8/16 beats means.2.In threshold confi...

ninad911 by Associate III
  • 2427 Views
  • 1 replies
  • 2 kudos

Multichannel ADC reading

Posted on August 16, 2016 at 18:31Hi,I am trying to read two adc channels number 10 and 11 with cubemx output. I can read the 10th channel with this code:HAL_ADC_Start(&hadc1);HAL_ADC_PollForConversion(&hadc1,10);value_adc=HAL_ADC_GetValue(&hadc1);H...

er3481 by Senior
  • 4999 Views
  • 9 replies
  • 1 kudos

STM32F746G- usb device mass storage with RTOS

Posted on July 19, 2016 at 16:03hi,      i have compiled and flashed the USB mass storage standalone project from STM32Cube_FW_F7_V1.1.0 STM32F746G MCU it works fine. but i have linked the same files with my project with RTOS now it showing in compu...

rajesh23 by Associate II
  • 3916 Views
  • 9 replies
  • 0 kudos

Boot into multiple main applications?

Posted on August 16, 2016 at 15:30I currently have my own bootloader running with a main application on a STM32F429ZIT.  The internal flash memory is broken down into 3 sections:1. Bootloader2. Main Application (Bank A)3. Temporary storage for new u...

Dual boot on STM32F427?

Posted on August 13, 2016 at 11:59Hello,I am rather confused, as I have read software dual boot was only possible in f7.But I recently came across dual bank boot options available on f4 : is it possible to dual boot on f4, in soft real-time?I use th...

maxzor by Associate II
  • 1335 Views
  • 2 replies
  • 0 kudos

HardFault with lwip+freeRTOS and STM32f745

Posted on April 18, 2016 at 11:02Hello, I'm using the lwip stack in combination with FreeRTOS for a http server (Netconn API) and modbus TCP (FreeModbus). I'm using the lwip stack and FreeRTOS from the ''STM32Cube_FW_F7_V1.3.0''. Evriting works grea...

twagner by Associate II
  • 3422 Views
  • 4 replies
  • 0 kudos

lwip+modbus/tcp

Posted on September 03, 2013 at 17:04hello every one .i tried to add modbus/tcp protocol in lwip(in webserver demo). i did it and it worked .but the problem is : if i use modbus/tcp protocol(via modbus poll software) it works correctly and if i use ...

USB-HID-HOST on STM32F407 / STM3240G EVAL

Posted on August 15, 2016 at 20:53Hello, I tried the example on the evaluation-board STM3240G-EVAL with the USB-HID-Host in Standalone mode HS and FS from the CubeF4 examples. The mice is recognised properly. The keyboard seems to work not properly....

ssl85 by Associate
  • 821 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.