2023-11-23 2:50 AM
Greetings,
trying to get a setup with stm32h753 running FreeRTOS and LwIP. One attempt in this journey was to take the example: How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community
Using the example code, I see one issue with the core lock - if the breakpoint in ethernetif.c line 987 is enabled I see the code suspends in places one would not expect it to suspend such as:
If I disable the breakpoint, ping works ok.
However even with this example the code quite often (if not always) gets stuck to Ethernet output, it seems that a packet comes down to ethernet low_level_output function, but never gets out to the cable. Suspecting it is a DMA issue, but had no luck locating the issue yet. Any ideas?
Thanks!
2023-12-02 12:36 PM
> There is no point in poking random features and doing other voodoo magic before the lower layers of code are fixed
Of course you're right. But these examples at least allow to verify PHY, clocks etc. and put some bits on the wire.
2023-12-02 12:48 PM
My point was about this:
In the meantime I have found out that, if the http headers for the http server are static then the files with static headers go through the stack and thus are received correctly. However for files that use dynamic http headers never leave the device.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.