2024-04-04 5:13 AM
Hi!I'm having some troubles in configuring the I2C bus on my STM32H747 evaluation board.
I've configured it in CubeMX as in the image below, using DMA buffer (rx and tx). Gpio pins are configured as open drain (no pull) and hardware is ok.
It seems like the peripheral is not correctly initialized because I can't see any toggle of SCL pin on my scope (both SCL and SDA go low during initialization but, after that, they don't move anymore).
Can someone help me please?
Thanks
Solved! Go to Solution.
2024-04-05 12:53 AM
Hello,
This is an example in Cube using I2C with DMA:
2024-04-04 5:34 AM
Hello,
Did you configure the pull-ups on SDA/SCL pins?
PS: you can inspire from this example provided in STM32CubeH7 package.
2024-04-04 5:45 AM
Thanks SofLit, I've already looked at that example, but it doesn't use DMA..
can you tell me if there is any command (about initialization) that I have to add to the code generated by the Cube? There is any command related to the timer enable?
Thanks
2024-04-05 12:53 AM
Hello,
This is an example in Cube using I2C with DMA:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.