STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32 uart receive error

Hello. I am getting fault error or uart_waitonflaguntiltimeout error when receiving data from UART via DMA on STM32F4 series microcontrollers when the power of the device on the other side is turned off. What could be the reason for this? What should...

Mixolyxo by Associate
  • 2237 Views
  • 3 replies
  • 0 kudos

Simple Ethernet test

Hi!I'm using a custom PCB with STM32F767 on it with LAN8742a for Ethernet communication.Just to mention, I'm totally new to Ethernet topics.I have already search for an very simple example on how to just test the connection from the STM to LAN8742a (...

Gregory3 by Associate III
  • 11553 Views
  • 5 replies
  • 0 kudos

Resolved! Bootloader UART: NACK to Write Command when try to write data to valid RAM memory addresses

To whom it may concern:We are currently developing a wearable devices, which is running on a STM32L031. In Bootloader mode, while I am trying to write data to vaild RAM address(0x20001F00), it returns NACK. Every step is followed instruction, but it ...

STM32CubeIDE vs mbed

Hello Everyone,I have STM32MP157F-DK2 board has an ARM Cortex-M4 chip that supports a frequency range of approx 209MHz. It takes about minimum 3.02 microseconds (Attached Screenshot) to achieve 40 clock pulses on this board. I also tried the STM32 Nu...

kundanJha by Associate II
  • 2485 Views
  • 0 replies
  • 0 kudos

STM32U575VIT6Q - USB CDC not enumerating

Hi All, We ran the example application code on our board with STM32U575VIT6Q and the USB CDC is not enumerating,whereas USB DFU mode is working when we trigger the boot0 button while powering on or resetting the devicehttps://github.com/STMicroelectr...

Resolved! STM32H745xi enter standby mode after power on 3 seconds

I use STM32H745xi discovery board. When i do some test, i download code that Cortex-m7 will enter standby mode after power on 3 seconds. And i set wrong wakeup pin(wakeup pin 1&not config PA0, it should be wakeu4). After power off and power on, i fin...

Jerry3 by Associate II
  • 2760 Views
  • 3 replies
  • 0 kudos

How to run BLE ota without optimization?

Hello,I'm currently working on an STM32WB55VCQ7 microcontroller using Visual Studio GDB. My project involves implementing a bootloader for over-the-air updates via BLE. I've made some progress by successfully flashing the example application located ...

emmaBK by Associate
  • 1034 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.