2024-07-19 5:57 AM
Hi,
I am using the STM32H745 and facing the following issue:
It appears that the DMAMUX is closely tied to both DMA controllers (DMA1 and DMA2). None of the available documents (es0445-stm32h745-errata, rm0399 - Reference Manual, en.STM32H7-DMAMUX, en.STM32H7-DMA) provide the required information on this behavior.
Is this the expected behavior? Are there any documents from STM32 that can justify this? some help would be greatly appreciated.
Thanks
2024-08-21 1:07 AM
Hello @shivashankarr
In order to reproduce the possible issue, could you please provide more details on your setting project if possible, attach your .ioc file/configuration?
2024-08-21 3:53 AM
Hello nouirakh,
Sorry, this is a non-IOC file setup, but I can provide detailed steps to reproduce the issue.
Case 1: Configure the ADC and DMA1 to interface with any sensor or memory, then reset DMA2 (in RCC->AHB1RSTR). Afterward, check the SFR register the DMAREQ_ID field in the DMAMUX_C0CR register will reset to 0.
Case 2: If you reset DMA2 (in RCC->AHB1RSTR) and then try to configure the ADC and DMA1, observe the SFR register (DMAREQ_ID field in the DMAMUX_C0CR register). It will not allow you to write the configuration.
BR
2024-08-30 6:45 AM
Hello @shivashankarr
I escalated this post internally and will be back to you with update.
Internal Ticket ID 189893 (It is an internal tracking number and is not accessible or usable by customers).
2024-11-12 12:21 AM
Hello @shivashankarr
After investigation, we confirm that this is the expected behavior. The reference manual will be updated to include this information for clarity.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.