2025-07-07 6:33 AM
I have constant measurement offset in Vbat internal channel from ADC3, ~30mV above the supplied value.
Vref calculated by macro:
__HAL_ADC_CALC_VREFANALOG_VOLTAGE((uint32_t)(measure->adcDataAverage[measureVref]) , ADC_RESOLUTION_16B);
i see offset of 4 mV above the configured 2.5V (reading is 2.504 - 2.505)
Vbat also calculated by macro:
__HAL_ADC_CALC_DATA_TO_VOLTAGE((uint32_t)(systemObj->dump[MIN_NET_ADDR_NUMBER - 1].measurement[measureObjVref][dbgObjectNameVoltage - dbgObjectNameCurrent]) , measure->adcDataAverage[measureVbat] , ADC_RESOLUTION_16B);
but offset is higher: 30mV above the input voltage.
i check with NUCLEO-H753ZI by run of STM32Cube\Repository\STM32Cube_FW_H7_V1.11.2\Projects\NUCLEO-H743ZI\Examples\ADC\ADC_InternalChannelConversion
and also observed offset around 20mV.
According to DS: https://www.st.com/resource/en/datasheet/stm32h743vi.pdf page 109, Vref has max.15 mv "spread", but the Vbat deviation is not specified.
Please advise.
Solved! Go to Solution.
2025-07-09 3:03 AM
Hello @AlexK
ADC conversions of channels to VrefInt and Vbat require minimum sampling time, specified in datasheet.
For STM32H742xx/43xx: tS_vrefint=4.3us min, tS_vbat = 9us min.
Sampling time depends on ADC kernell clock frequency (from RCC and ADC config) and ADC channel sampling time config.
Could you check your configuration ?
ADC channel to Vbat accuracy:
Vbat is measured through a resistor ladder, tolerance is specified in datasheet : table "VBAT monitoring characteristics"
For STM32H742xx/43xx: +-10%
2025-07-09 3:03 AM
Hello @AlexK
ADC conversions of channels to VrefInt and Vbat require minimum sampling time, specified in datasheet.
For STM32H742xx/43xx: tS_vrefint=4.3us min, tS_vbat = 9us min.
Sampling time depends on ADC kernell clock frequency (from RCC and ADC config) and ADC channel sampling time config.
Could you check your configuration ?
ADC channel to Vbat accuracy:
Vbat is measured through a resistor ladder, tolerance is specified in datasheet : table "VBAT monitoring characteristics"
For STM32H742xx/43xx: +-10%
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.