2024-09-15 11:55 PM - last edited on 2024-09-16 3:04 AM by mƎALLEm
Hello everyone, i am trying to configure one STM32H723 as TCP Client and another as TCP Server. I am very new to networking. I used the example project in this github link and didnt change anything except IP addresses and MAC addresses https://github.com/stm32-hotspot/STM32H7-LwIP-Examples/tree/main/STM32H723_Nucleo_ETH.
I am having problem in the client side TCP_Connect function. The function calls ip_route function and this function returns -4(Routing Problems). While debugging i saw that my device doesnt get into this loop inside ip4_route function which i believe indicates i dont have any network interfaces.
NETIF_FOREACH(netif) {
/* is the netif up, does it have a link and a valid address? */
if (netif_is_up(netif) && netif_is_link_up(netif) && !ip4_addr_isany_val(*netif_ip4_addr(netif))) {
/* network mask matches? */
if (ip4_addr_netcmp(dest, netif_ip4_addr(netif), netif_ip4_netmask(netif))) {
/* return netif on which to forward IP packet */
return netif;
}
/* gateway matches on a non broadcast interface? (i.e. peer in a point to point interface) */
if (((netif->flags & NETIF_FLAG_BROADCAST) == 0) && ip4_addr_cmp(dest, netif_ip4_gw(netif))) {
/* return netif on which to forward IP packet */
return netif;
}
}
}
However i didnt change the code so in lwip.c there is a netif structure instance called gnetif. For further explanation,
this is IP address settings for my client:
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 1;
IP_ADDRESS[3] = 10;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 192;
GATEWAY_ADDRESS[1] = 168;
GATEWAY_ADDRESS[2] = 1;
GATEWAY_ADDRESS[3] = 1;
and this is IP address settings for my server:
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 1;
IP_ADDRESS[3] = 20;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 192;
GATEWAY_ADDRESS[1] = 168;
GATEWAY_ADDRESS[2] = 1;
GATEWAY_ADDRESS[3] = 1;
2024-09-16 6:33 AM
Hello @mazotcu16 ,
Please modify the IP address in the StartDefaultTask function at line 324, specifically the line:
IP4_ADDR(&remote_addr, 192, 168, 1, 1);so that it matches the IP address of your server.
With Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.