2021-12-06 9:15 AM
Currently when I unplug my Nucleo Board from my computer, my computer blue screens with a "SYSTEM_THREAD_EXCEPTION_NOT_HANDLED" error. Any ideas on what would cause this?
It happens every time I unplug the board, even if all I do is plug it in, then unplug it right away.
Solved! Go to Solution.
2021-12-08 4:41 AM
Hi Pavel,
When I tried this, windows crashed on the spot, with the same error as I see when physically unplugging the hardware.
2021-12-08 5:35 AM
Thanks to all that replied, I have found an answer.
The issue was that company policy around USB devices would not agree with the nucleo board being mounted as a USB device. We do not use the USB storage on the nucleo board, so within the STM32Cube Programmer application, there is an option to do a firmware upgrade for the ST-LINK debugger. When doing the upgrade, you can change its type to remove the Mass Storage option.
This fixed the issue!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.