2024-05-17 4:27 AM
Hi,
HAL and LL DAC configuration structure and its parameters naming can be confusing. Reference manual claims that DAC "mode" (register ADC->MCR, bits 0..2 or 16..17) can be in one of following four combinations when not used sample and hold mode:
0 -> DAC channel2 is connected to external pin with Buffer enabled
1 -> DAC channel2 is connected to external pin and to on chip peripherals with buffer enabled
2 -> DAC channel2 is connected to external pin with buffer disabled
3 -> DAC channel2 is connected to on chip peripherals with Buffer disabled
These combinations coherent but HAL DAC init struct offers up to six conbinations (Enable/Disable buffer times Internal/External/both connections). Some of them are not accesible. I've listed following configurations:
a) - OK
DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
Resulting configuration: 0 -> DAC channel2 is connected to external pin with Buffer enabled
b) - Misleading
DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_INTERNAL;
Resulting configuration: 1 -> DAC channel2 is connected to external pin and to on chip peripherals with buffer enabled
c) - OK
DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_BOTH;
Resulting configuration: 1 -> DAC channel2 is connected to external pin and to on chip peripherals with buffer enabled
d) - OK
DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
Resulting configuration: 2 -> DAC channel2 is connected to external pin with buffer disabled
e) - OK
DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_INTERNAL;
Resulting configuration: 3 -> DAC channel2 is connected to on chip peripherals with Buffer disabled
f) - Misleading
DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_BOTH;
Resulting configuration: 2 -> DAC channel2 is connected to external pin with buffer disabled
Also LL API have misleading parameter naming:
a) - OK
OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE;
OutputConnection = LL_DAC_OUTPUT_CONNECT_GPIO;
Resulting configuration: 0 -> DAC channel2 is connected to external pin with Buffer enabled
b) - Misleading
OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE;
OutputConnection = LL_DAC_OUTPUT_CONNECT_INTERNAL;
Resulting configuration: 1 -> DAC channel2 is connected to external pin and to on chip peripherals with buffer enabled
c) - OK
OutputBuffer = LL_DAC_OUTPUT_BUFFER_DISABLE;
OutputConnection = LL_DAC_OUTPUT_CONNECT_GPIO;
Resulting configuration: 2 -> DAC channel2 is connected to external pin with buffer disabled
d) - OK
OutputBuffer = LL_DAC_OUTPUT_BUFFER_DISABLE;
OutputConnection = LL_DAC_OUTPUT_CONNECT_INTERNAL;
Resulting configuration: 3 -> DAC channel2 is connected to on chip peripherals with Buffer disabled
You probably should enhance comment of structs
LL_DAC_InitTypeDef
DAC_ChannelConfTypeDef
to cover this confusions. Or/And change macros names. Or better change struct structure to correspond reference manual with four legal combinations.
Solved! Go to Solution.
2024-05-21 12:35 AM
Hello @Michal Dudka ,
Thank you for having reported your feedback.
I highlighted this request (via the internal ticket number: 181777) to our development team to be analyzed.
(PS: Internal ticket number 181777 is an internal tracking number and is not accessible or usable by customers).
2024-05-21 12:35 AM
Hello @Michal Dudka ,
Thank you for having reported your feedback.
I highlighted this request (via the internal ticket number: 181777) to our development team to be analyzed.
(PS: Internal ticket number 181777 is an internal tracking number and is not accessible or usable by customers).
2024-06-05 1:20 AM
Hi @Michal Dudka,
About your reported cases Misleading mentioned in the description:
"b)": not a problem: connection internal requested is provided (with connection to external pin in addition. If needed, can be disconnected from pin by setting GPIO in digital mode)
"f)": indeed this is a problem because connection DAC_CHIPCONNECT_BOTH requested is not provided, connection is only on GPIO(DAC_CHIPCONNECT_EXTERNAL)
About proposal "...change struct structure to correspond reference manual with four legal combinations": the problem is that depending of mode normal or sample & hold, these 4 combinations are different.
The 3 parameters {mode; output buffer; connection} are managed in unitary way in drivers:
* @note On this STM32 series, output connection depends on output mode
* (normal or sample and hold) and output buffer state.
* - if output connection is set to internal path and output buffer
* is enabled (whatever output mode):
* output connection is also connected to GPIO pin
* (both connections to GPIO pin and internal path).
* - if output connection is set to GPIO pin, output buffer
* is disabled, output mode set to sample and hold:
* output connection is also connected to internal path
* (both connections to GPIO pin and internal path).
We propose to update HAL DAC driver:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.