2022-08-11 6:07 AM
I have flashed the firmware into flash memory using i2c application programming.when the controller is booting from flash memory,i can see the uart console logs .
I have configured the PB6 and PB7 pins are i2c pins.I set the clock speed to fast mode using stm32cubemx generator.I2c own address bit also set with 7bit I2C address << 1.But i2c is not detected.Is there any configuration missing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.