2019-09-16 6:35 AM
We developed a product which uses STM32F series and everything works fine. For some reason, we need to swap the F serie to G serie for future products.
Unfortunately, we do not manage to flash the virgin device (STM32G070CBT6) through USART1 (PA9/PA10) using stm32flash. The error message says "failed to init device". We also tried to write to the option bytes (address 0 x 1FFF 7800) so that the boot is targeting the System Memory, but doing this results in the same error message. So here are the questions:
Any other suggestions that might alleviate the problem?
Thanks a lot in advance
Astrid
2019-10-08 4:21 AM
Hello,
Not that many answers on this board.
Thanks
Astrid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.