STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am trying to program the main memory using Demonstrator GUI application. But i am getting below attached error. PLease help me to get use of system bootloader.

i am using Neucleo L4R5ZIP development board. I am planning to use System Bootloader. I have enabled the system bootloader by enabling the BOOT0 pin and BOOT1 Register configuration. Through LD3 LED, i can able to verify the system Bootloader started...

Kmoor by Associate
  • 972 Views
  • 0 replies
  • 0 kudos

Is there an STM32 USB device Iscochronous In Example?

I am in search of a USB example class that uses Isochronous streaming from the device (In Endpoint). I see there is an audio example that is an Out Endpoint (receives data from the host). Is there an example project that streams data from the devic...

AHats by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos

STM32 VID/PID

We are considering changing our products to use STM32. It's Arduino based and using Atmel products now. To be able to chose a suitable STM32 we would need to adapt the USB interface instead of using an FTDI chip. But from posts I read here I can't se...

Are CHM help files abandoned? Any substitute?

I use STM32Cube_FW_F0_V1.6.0\Drivers\STM32F0xx_HAL_Driver\STM32F070xB_User_Manual.chm for help. These files are from 2016 and seem abandoned. Are there newer versions to download or is there online version (they are compiled HTMLs) of them with the...

0690X00000A9jwrQAB.png

How can I interface and use an electret condensor Microphone with STM32F407 discovery board to record and playback audio ?

I have already searched the whole internet and also tried this Cube repository for Audio playback and record from Github and ReadMe pdf file from inside CubeMX repository, link of Github code and uploaded README pdf file is available below.I got it s...

SDube.2 by Associate
  • 1305 Views
  • 0 replies
  • 0 kudos

Resolved! DP ALWAYS Pulled High (UP)?

Hello All,I am currently working on a USB device that supplies power (Chip = STM32F765). I am attempting to have this device be connected and unrecognized while in stop or standby mode and I am running into the unfortunate fact that the DP line has a...

ZThat by Senior
  • 4305 Views
  • 6 replies
  • 0 kudos

stm32f1 fw package 1.70 SPI bug

Im using stm32f103RB on nucleo64 board, to read SPI sensor with half duplex SPI master mode.SPI blocking recive function do not disable SPI properly, it should disable it and then finish recive one more time, as user manual RM0008 specify(25.3.8), bu...

VLuky by Associate II
  • 2201 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.