2023-11-05 4:05 PM
Hey everyone, I have developed a circuit board with STM32G030. I use the STOP 1 mode to save power, the device wakes up on a pin change interrupt.
Sometimes the current consumption in STOP 1 mode is around 1,2mA higher mode than normal (3uA) but lower than run mode(2,5mA) and the MCU does not wake up anymore. The same in Standby Mode.
I can´t find the reason, maybe someone has an idea.
Here is my STOP Mode function:
void StopMode(void)
{
LED_On(OFF);
I2C_On(OFF);
MOT_EN(OFF);
//DisableDebugger();
//disablePeripherie();
HAL_SuspendTick();
sleep = 1;
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); //Stop 1
SystemClock_Config();
HAL_ResumeTick();
USR_LED_On(1);
LED_On(ON);
I2C_On(ON);
MOT_EN(ON);
}
2023-11-05 5:11 PM
After some testing I figured out that the problem is only present when I run the Timer 3 with PWM generation before going to sleep. The Errata sheet mentions something but my HSI_DIV is set to [00]
code out of main.c:
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
STM32G030x6/x8 device errata:
2.2.6 Wakeup from Stop not effective under certain conditions
Description
With the HSI clock divider bitfield HSIDIV[2:0] set to a value different from 000, the device fails to enter Stop
mode when SYSCLK is set to HSE clock.
With the HSI clock divider bitfield HSIDIV[2:0] set to a value different from 000, peripherals with clock request
capability fail to wake the device up from Stop modes.
Workaround
None.
2024-02-27 4:20 AM
Hello JakobB,
could you figure out your problem ?
We have a similar issue using an STM32G0B1 ...
Best regards,
lakeroe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.