2020-12-17 9:16 PM
Hi,
I am using a STM32F769I Disco board for testing the speeds of the High Speed USB as a MSC. At present, the system is working as expected as a MSC over uSD. However, my concern is with respect to the read write speed of 2.5MB/s which seems to be very low for High Speed Applications. I have used the HAL Libraries and ST provided Examples for the firmware.
At the uSD side, I am able to get a speed of 6 MB/s, but when the read write is over HS-USB as MSC, the speed I get is around 2.5MB/s.
Would be very helpful if any one can provide any insights.
Thank You,
Amit K
2020-12-24 10:00 PM
I have similar issue with UVC class devices.
In my project I met the same bandwidth limit
In my case this limit 10 megabit per second ( same as 2.5 megabyte per second )
USB HS has 125 uS microframe duration
isochronous max packet size is 1024 bytes
If to send one packet per microframe - we exactly meet the limit 2.5 MB/s
USB HS protocol has an option to send up to 3 packets per microframe which can increase bandwidth up to 3 times
However, it requires some additional coding ( i think )
2020-12-25 9:32 PM
Hi YKorc,
So as per your analysis, the speed issue is at the USB side of the device? If I am not wrong, then this will be the same speed one can achieve if writing directly to a Pen drive as a Host.?
2021-07-19 6:50 AM
hi @YKorc.1
I am interested in implementing UVC device on STM32F7- that is, I need my device to act as a web cam.
CubeMx doesn't seems to support UVC and I wasn't able to find any examples.
Can you please give me some pointers how you did it?
thanks,
Arnon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.