2025-04-02 1:42 AM
Hi, I am triyng to develop custom bootloader. My application address is 0x08180000 and bootloader address is 0x08000000. I can start with the bootloader and jump to the application successfully.
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_UART_Transmit(&huart1, (uint8_t *)"HELLO", strlen("HELLO"), HAL_MAX_DELAY);
HAL_Delay(1000);
}The application send "HELLO" message over UART. but when I set MPU configurations I cant see the message coming from application. Here is my MPU configuration.
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x08000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x08180000;
MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x20000000;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
Why I get failure when I try to jump application? What must the MPU configuration be?
This is my application flash.ld file
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x08180000, LENGTH = 512K
}This is my bootloader flash.ld file
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1536K
}
Can you help me to configure MPU? The reason I am setting MPU is I need to use ethernet in bootloader. I need to use MPU configurations If I want to use ethernet in stm32f767zi. And I must use it. Can you help me? @mƎALLEm @Andrew Neil @TDK can you help me, guys?
Solved! Go to Solution.
2025-04-02 11:30 PM
Sorry guys, it is not about MPU configuration; I got the failure because of the system PLLQ clock mismatch between bootloader and application. You should be careful about MPU region and clock if you are facing a problem like me.
2025-04-02 11:30 PM
Sorry guys, it is not about MPU configuration; I got the failure because of the system PLLQ clock mismatch between bootloader and application. You should be careful about MPU region and clock if you are facing a problem like me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.