2017-05-21 4:36 AM
Hello,
I want to create a webserver application, and I want my html file modified seperately. So I think that saving my web files (including .html, .css and .js files) into SD card I a good solution, So whenever I want to modify my website, I just need to edit web files and put them into SD card.
I read a lot about lwIP and FatFs package but I still dont know how to figure it out.
Can any one expert on this field give me an example project like that? any IDE project is OK. Or I just need to be guided to configure the STM32cubeMX, and create a simple webserver saved on SD card.
Thank you very much
#fatfs #sd-card #web-server #lwip2017-05-24 7:39 AM
Hi Hoang,
the STM32Cube provides a http server application based on the LwIP API.Have a look at the project:
Projects\STM32756G_EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS
the LwIP comes with a builtin http server, the server is expecting the html pages in the file 'fsdata_custom.c' when the lwip config flag HTTPD_USE_CUSTOM_FSDATA is defined.
for the aforementioned project, the actual html pages and data are under 'Projects\STM32746G-Discovery\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS\Fs'
you can use any binary dump tool,
https://kent.dl.sourceforge.net/project/bin2header/current/bin2header_0.0.1_portable-win32.zip
for example, to generate your own 'fsdata_custom.c' from your webpages.Could you please try and let us know whether it suits your needs?
regards
Haithem.
2017-05-24 10:49 AM
Hi Haithem, thanks for replying me, that's very helpful, I will try this example.
But I have two question:
Is there any way that I can send my web directly to the client, without converting it into the fsdata_custom file?
I read about TFTP, can I use this interface to do some thing like on-the-air update for my web server?. For example I just need to modified my web files (including css,js or cgi files) on my PC and send them to the kit via TFTP interface(with or without converting to fsdata file is all OK), after that the web server will display with the new updates.
If any of my questions is possible, could you show me a brief guide to do it?
Many thanks no matter if you could or couldn't help me this
2017-05-30 5:35 AM
Hi Hoang
I'm working on a small project that show logs file using lwip. It's possible to read custtom pages/files from sdcard by using
LWIP_HTTPD_CUSTOM_FILES
LWIP_HTTPD_DYNAMIC_FILE_READvariables. Then you need to implements 3 custom methods :
int fs_open_custom(struct fs_file *file, const char *name);
void fs_close_custom(struct fs_file *file); int fs_read_custom(struct fs_file *file, char *buffer, int count);I'm still working on it, but this is the starting point if you want to use lwip+sd card without using freertos
Andrea
2017-06-01 2:02 AM
Thank andrea,
That's very helpful. I will try your suggestion.
Have a good day
2017-06-05 12:44 PM
here is my starting code:
//open custom file
int fs_open_custom(struct fs_file *file, const char *name) {//open log file
if(strncmp_url(name,'/log_file.txt',13)>0) { file->data = 'buffer_open_custom'; file->len = 1000; file->index = 0; file->pextension = NULL; file->is_custom_file = 1; //0 if unable to open return 1; }}//read file and fill 'buffer' step by step by 'count' bytes amount
int fs_read_custom(struct fs_file *file, char *buffer, int count) { int read = 0; if (file->index < file->len) { read = 100; file->is_custom_file = 1; buffer = 'buffer_read_custom'; } else { //end reached read = FS_READ_EOF; } return read;}void fs_close_custom(struct fs_file *file){
//close file
//f_close(&fileOpen);}
fs_open_custom works ok and the first part of the page is correctly loaded, then fs_read_custom is called 10 times before return FS_READ_EOF but only the first call appends to the buffer 'buffer_read_custom' string, next calls append only part of 'fsdata_custom.c' file. Any idea about this behavior? This is only a proof of concept example. I just need to test this code works correctly
2017-06-05 1:18 PM
Is it so that there is no example project or code for the SD card in the 746 Discovery? Even though there SD drive included. Probably many of us could one, me included.
2017-06-05 3:24 PM
read/write from to the sd card is quite simple. My problem is to stream huge custom log files stored on usb to port 80 by using lwip. I need to solve issue with buffer of fs_read_custom method...
2017-06-05 7:37 PM
STM32Cube_FW_F7_V1.7.0/Projects/STM32746G-Discovery/Examples/BSP
and
STM32Cube_FW_F7_V1.7.0/Projects/STM32746G-Discovery/Applications/Display/LTDC_PicturesFromSDCard
both contain example code for SD
2017-06-06 2:07 AM
thank you but my problem is on lwip side, not sd side. I need to show custom page/log file using lwip webserver...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.