2017-06-12 8:14 AM
I'm working on the audio example and I've made it work with Audio Class 2.0. Device enumerates and ISO packets are received.
However when I decided to enable DMA for better performance the TX line is not working. Device receives Setup packets, but cannot transmit.
In the generated from CubeMX code I saw the following:
// Be aware that enabling DMA mode will result in data being sent only by multiple of 4 packet sizes. This is due to the fact
// that USB DMA does not allow sending data from non word-aligned addresses.
Does somebody knows how 'large' is one packet or where that is defined?
Anyone bumped into that problem?
Using:
- System Workbench for STM32
- STM32Cube_FW_F7_V1.7.0
#stm32-usb-dma #stm32-usb #stm32 #stm32f72020-07-14 4:27 AM
Hello, Momchil Stanchev!
I am working on Audio Class 2.0 device but could not get it working yet. Could you please share your source code regarding USB Audio Class 2.0?
2020-07-28 4:42 AM
Hi, I will try it in the next few days, too.
It says "... data being sent only by multiple of 4 packet sizes." So what is your packet size?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.