2013-03-11 11:22 PM
I have got the USB Audio Device example working on the stm32f4discovery board . When connected to my laptop via usb , the board can be recognized as an speaker. There is audio output from the headphone when play music on my laptop .However , the audio output is really funny , women sounds like man in the output of the board .
It seems that the I2S output clock frequency of the dicovery board is slightly higher than the audio sample rate of the laptop output . Is there a way to make the I2S output clock frequency the same with the audio sample rate of the laptop output? ----------------------------------- I have changed the I2S input clock from 3840000 to 86000000 by generating another system_stm32f4xx.c file.It is much better now , still not perfect. #stm32f4discovery-usb-audio2014-03-05 12:23 AM
I have the STMF4 Discovery working as USB Audio Sound Card.
Project and few details are here: www.tjaekel.com Best regards TorstenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.