2012-12-25 8:46 PM
hi
how can I get high speed USB interface to host a device on STM32F4discovery? would i have to remove component from the kit OR just add additional PHY? #high-speed-usb #usb-otg #cpen #otg_hs #highspeed #metoo-not-quite #host_ctrl_xfer #vbus2013-01-14 1:30 AM
i have managed to run ULPI High speed interface with external EVAL board of USB3300 .
I am not able to modify the code available in audio record play back (for STM32f4discovery) to HIGH SPEED, I have made the important changes , but what i am missing here?. i have changed the OTG_FS to OTG_HS and define ULPI etc... I get to the point that Enumuraton is not done, I didnt get USBH_OK from function USBH_Handle_ENUM...(). and my Code get continuously pooling through HOST_CTRL_XFER after failed enumeration.2013-01-23 9:08 PM
i am using USB3300 SMSC eval board. I am able to run high speed ULPI interface with STM32F4 Discovery using MSC high speed example for STM324xx boards. I get a little highspeed than fullspeed. the ULPI is running well.
1=>I can write files to USB using ULPI highspeed interface, but I can't achieve High Data rate as expected. 2=> the speed get more lower about after 1000 files written, I am using character array of length 5 , name={'0','0','0','0','0'} and after when name={'0','1','0','0','0'} the speed get lower? why is that so? is due to the long file name I am using or what else? {if i refresh the name to 0,0,0,0,0 the speed get to its original} thanks2013-03-18 6:03 PM
Hey, i got question. How you managed to fix this problem when program was continuously pooling through HOST_CTRL_XFER after failed enumeration? I've got the same problem and i can't find solution.
2013-03-18 6:19 PM
Also I used MSC example for STM3210C-EVAL borad.
2013-03-19 6:51 AM
Also I used MSC example for STM3210C-EVAL borad.
So a bit off-topic then, perhaps a new thread with details of YOUR issue, and compiler settings, etc, might be a better route.2013-03-21 11:12 AM
Ok, I started new thread in
https://my.st.com/public/STe2ecommunities
>https://my.st.com/public/STe2ecommunities/mcu
> [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=0]STM32 >STM23F105RC USB OTG problem
link: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM23F105RC%20USB%20OTG%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fm...2013-03-24 2:43 PM
Hey, tech.haris can you just tell me what did you do do deal with this continuous pooling through HOST_CTRL_XFER after failed enumeration? I know it might not relate at all to my problem, but since nobody want to say something I'll be very glad to get some hint.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.