2016-06-15 7:15 AM
Hello,
i would like to know whether i can program STM32F446RE -Nucleo Board using standard library's? and if yes can i please have some examples using standard library.I searched online but i did not get any further information. i want to program STM32F446RE -Nucleo Board for CAN BUS: Thanks in advance! #stm32f4-can-tx-rx #stm32-standard-peripheral-librar #stm32-nucleo #stm32f4-can-tx-rx #!stm32f42016-06-15 7:31 AM
Hi saraf.ninad.001,
All STM32 boards can be programmed either using HAL library or Standard library. For STM32F4 devices, you find last version of the Standard library package at this . -Hannibal-2016-06-15 8:32 AM
The SPL can certainly be used for those boards/chips, many of the existing examples can be ported to the board, which shouldn't be too difficult, just pay attention to the pins, clocks, etc.
2016-06-20 12:17 PM
Thank you so much for the link. But to program STM32F446RE-Nucleo board i require library of STM32F446RE-Nucleo board board. On the link i am unable to find library fr the above mentioned board. can someone please provide me a link for STM32F446RE-Nucleo board library. My IDE is Atollic TrueSTUDIO:
Thanks in advance!2016-06-20 12:34 PM
The F4 DSP library is usable with the F446RE part, as are a whole range of F4 parts.
There is not a specific ''Nucleo-F446RE'' library/example, one would simply need to construct a project on the chosen IDE and select the STM32F446 as the Target device. Suggest you try something simple like blinking an LED/GPIO or outputting to the serial port via a USART.Sorry, I'm not using Atollic.2016-06-22 11:02 AM
I am trying to program on IDE: ATTOLLIC TRUE STUDIO by selecting the desired board STM32F446RE-Nucleo and importing the library files from the link given by you. But after building the project there are problems linking the library files to the main project. that is example in the instruction 'GPIO_LED.GPIO_Pin = GPIO_Pin_12;' the program should link me to GPIO library when i will click on GPOI_Pin but it is not linking me to the library. To conform if it is happening for all other boards i created new project for STM32F4_Discovey board, for which the library files were automatically downloaded it is working.
Can any one help me with this problem please.2016-06-22 12:05 PM
Consider how your tools would work if this were a fully custom board no one had ever seen before? Perhaps you should look at doing this from a chip perspective rather than a board one?
You could also use a NUCLEO-401RE as a target board, and then change the Target CPU, or just run the part at 84 MHz until you get sufficiently familiar with your chosen tool chain. Seek support/training from Atollic.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.